InactiveItemCount
Description
This counter indicates the number of items with inactive status.
TIP:
InactiveItemsCount provides a real-time item count rather than an accumulated value since the service started. The value will change as items are set as active or inactive.
Location
- FactoryTalk Diagnostics Counter Monitor > System Diagnostics > localhost > FactoryTalk Linx Gateway OPC DA Server > DaClient_X> GroupX
Value
- Type: Unsigned integer
- Source: This value is generated by the FactoryTalk Linx Gateway OPC DA server.
- Updates: This value increases when the OPC DA client sets an item as inactive and decreases when the client sets it as active.
- Reset: This value resets when you reset the service or restart the computer.
Provide Feedback