ActiveItemsCount

Description
This counter indicates the number of items with active status.
TIP:
ActiveItemsCount provides a real-time item count rather than an accumulated value since the service started. The value will change as items are set as active or inactive.
Location
  • FactoryTalk Diagnostics Counter Monitor > System Diagnostics > localhost > FactoryTalk Linx Gateway OPC DA Server > DaClient_
    X
    > Group
    X
Value
  • Type: Unsigned integer
  • Source: This value is generated by the FactoryTalk Linx Gateway OPC DA server.
  • Updates: This value increases when the OPC DA client sets an item as active and decreases when the client sets it as inactive.
  • Reset: This value resets when you reset the service or restart the computer.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal