Sync Write calls
Description
This counter indicates the number of requests the OPC DA client made to edit data synchronously. The client waits for the server to provide the requested data before proceeding.
Location
- FactoryTalk Diagnostics Counter Monitor > System Diagnostics > localhost > FactoryTalk Linx Gateway OPC DA Server > DaClient_X
Value
- Type: Unsigned integer
- Source: This value is generated by the FactoryTalk Linx Gateway OPC DA server.
- Updates: This value increases when an OPC DA client requests to edit data synchronously.
- Reset: This value resets when you reset the service or restart the computer.
Provide Feedback