Name

Description
The value indicates the name of the OPC DA client.
Location
  • FactoryTalk Diagnostics Counter Monitor > System Diagnostics > localhost > FactoryTalk Linx Gateway OPC DA Server > DaClient_
    X
Value
  • Type: String
  • Source: This value is generated by the FactoryTalk Linx Gateway OPC DA server.
  • Updates: This value is loaded when the client connects to the server.
  • Reset: This value will be retrieved when you reset the service or restart the computer.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal