Failed Writes
Description
This counter indicates the number of times when the write requests from the OPC DA client are unsuccessful. The FactoryTalk Diagnostics will show the client, group, and item name that failed.
Location
- FactoryTalk Diagnostics Counter Monitor > System Diagnostics > localhost > FactoryTalk Linx Gateway OPC DA Server > DaClient_X
Value
- Type: Unsigned integer
- Source: This value is generated by the FactoryTalk Linx Gateway OPC DA server.
- Updates: This value increases when an OPC DA client fails to edit the data item.
- Reset: This value resets when you reset the service or restart the computer.
Provide Feedback