Failed to Add Items

Description
This counter indicates the number of items that the OPC DA clients are unable to add.
The FactoryTalk Diagnostics Event Log will show the items that are unable to be added. The event log messages may originate from either "FactoryTalk Linx Gateway" or "FactoryTalk Service."
Location
  • FactoryTalk Diagnostics Counter Monitor > System Diagnostics > localhost > FactoryTalk Linx Gateway OPC DA Server > DaClient_
    X
Value
  • Type: Unsigned integer
  • Source: This value is generated by the FactoryTalk Linx Gateway OPC DA server.
  • Updates: This value increases when an OPC DA client fails to add an item.
  • Reset: This value resets when you reset the service or restart the computer.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal