Failed Async Completes

Description
This counter indicates the number of times when ASync Read Complete Calls and ASync Write Complete Calls fail.
If the value in this counter is incrementing, it indicates that a client connection has failed. A FactoryTalk Diagnostics Message is also generated. Verify all client connections.
Location
  • FactoryTalk Diagnostics Counter Monitor > System Diagnostics > localhost > FactoryTalk Linx Gateway OPC DA Server > DaClient_
    X
Value
  • Type: Unsigned integer
  • Source: This value is generated by the FactoryTalk Linx Gateway OPC DA server.
  • Updates: This value increases when the OPC DA server fails to complete an asynchronous read operation or an asynchronous write operation.
  • Reset: This value resets when you reset the service or restart the computer.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal