Add Item calls
Description
This counter indicates the number of requests the OPC DA client made to add an item.
TIP:
An OPC DA client can add multiple items using a single Add Item call.
Location
- FactoryTalk Diagnostics Counter Monitor > System Diagnostics > localhost > FactoryTalk Linx Gateway OPC DA Server > DaClient_X
Value
- Type: Unsigned integer
- Source: This value is generated by the FactoryTalk Linx Gateway OPC DA server.
- Updates: This value increases when an OPC DA client requests to add an item.
- Reset: This value resets when you reset the service or restart the computer.
Provide Feedback