Sub_Topic
Description
This counter indicates the user-assigned topic name, which identifies the information channel from which payload data is received.
You can configure the topic name in .
FactoryTalk Linx Gateway
Configuration > MQTT > MQTT Client > MQTT Dataset > Dataset PropertiesLocation
- FactoryTalk Diagnostics Counter Monitor > System Diagnostics > localhost >FactoryTalk Linx GatewayMQTT Server > [Client ID] > [Dataset Name]
Value
- Type: String
- Source: This value is generated by theFactoryTalk Linx GatewayMQTT service.
- Updates: This value updates when the configuration changes in the MQTT dataset.
- Reset: This value resets when you reset the service or restart the computer.
Provide Feedback