Sub_Success to Write Data
Description
This counter indicates the total number of dataset tags that the
FactoryTalk Linx Gateway
MQTT subscriber writes to the FactoryTalk
destinations. FactoryTalk
destinations can be controllers connected
through FactoryTalk Linx
, OPC UA servers connected through FactoryTalk Linx
OPC UA Connector, FactoryTalk View SE
Tag Services
connected through an OPC DA server.Location
- FactoryTalk Diagnostics Counter Monitor > System Diagnostics > localhost >FactoryTalk Linx GatewayMQTT Server > [Client ID] > [Dataset Name]
Value
- Type: 64-bit signed integer
- Source: This value is generated by theFactoryTalk Linx GatewayMQTT service.
- Updates: This value increases when the MQTT subscriber successfully writes a dataset tag to the controllers.
- Reset: This value resets when you reset the service or restart the computer.
Provide Feedback