Sub_Received Messages

Description
This counter tracks the total number of MQTT messages received by the
FactoryTalk Linx Gateway
MQTT subscriber from the broker that matches its configuration in
FactoryTalk Linx Gateway
.
Location
  • FactoryTalk Diagnostics Counter Monitor > System Diagnostics > localhost >
    FactoryTalk Linx Gateway
    MQTT Server > [Client ID] > [Dataset Name]
Value
  • Type: 64-bit signed integer
  • Source: This value is generated by the
    FactoryTalk Linx Gateway
    MQTT service.
  • Updates: This value increases when the MQTT subscriber successfully receives an MQTT message from the broker that matches its configuration.
  • Reset: This value resets when you reset the service or restart the computer.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal