Sub_Received Items
Description
This counter tracks the total number of dataset tags received by the
FactoryTalk Linx Gateway
MQTT subscriber from the broker that matches its
configuration.Location
- FactoryTalk Diagnostics Counter Monitor > System Diagnostics > localhost >FactoryTalk Linx GatewayMQTT Server > [Client ID] > [Dataset Name]
Value
- Type: 64-bit signed integer
- Source: This value is generated by theFactoryTalk Linx GatewayMQTT service.
- Updates: This value increases when theFactoryTalk Linx GatewayMQTT subscriber successfully receives a dataset tag from the broker that matches its configuration.
- Reset: This value resets when you reset the service or restart the computer.
Provide Feedback