Sub_QoS
Description
This value indicates the level of guarantee for delivering messages between the MQTT
subscriber and the broker.
You can configure this setting in .
FactoryTalk Linx Gateway
Configuration > MQTT > MQTT Client > AdvanceThe MQTT provides three levels of QoS (Quality of Service):
- At most onceThe message is delivered at most once. There is no confirmation of delivery or retries.
- At least onceThe message is delivered at least once. The publisher expects an acknowledgment of receipt from the broker. If the publisher does not receive an acknowledgment within a specified period, it will resend the message.
- Exactly onceThe message is delivered exactly once, involving a four-step handshake process to achieve message delivery and acknowledgment.
Location
- FactoryTalk Diagnostics Counter Monitor > System Diagnostics > localhost >FactoryTalk Linx GatewayMQTT Server > [Client ID] > [Dataset Name]
Value
- Type: String
- Source: This value is generated by theFactoryTalk Linx GatewayMQTT service.
- Updates: This value updates when the configuration changes in the MQTT client.
- Reset: This value resets when you reset the service or restart the computer.
Provide Feedback