Sub_Payload Format
Description
This value indicates the format in which the payload of messages is structured.
- FactoryTalk Optix Format
- Rich Format
- Flat Format
You can configure this setting in .
FactoryTalk Linx Gateway
Configuration > MQTT >
MQTT Client > AdvanceFor more information on the payload format, see .
FactoryTalk Linx Gateway
HelpLocation
- FactoryTalk Diagnostics Counter Monitor > System Diagnostics > localhost >FactoryTalk Linx GatewayMQTT Server > [Client ID] > [Dataset Name]
Value
- Type: String
- Source: This value is generated by theFactoryTalk Linx GatewayMQTT service.
- Updates: This value updates when the configuration changes in the MQTT client.
- Reset: This value resets when you reset the service or restart the computer.
Provide Feedback