Sub_Only Write Change Value
Description
This counter indicates whether the
FactoryTalk Linx Gateway
MQTT subscriber writes
data to the FactoryTalk
destinations only when the data has changed. FactoryTalk
destinations can be controllers connected through FactoryTalk Linx
, OPC UA servers connected through FactoryTalk Linx
OPC UA Connector, FactoryTalk® View Site Edition (SE)
Tag Services connected through
an OPC DA server.- Yes: The subscriber updates theFactoryTalkdestinations only when there are modifications.
- No: The subscriber writes all data values, regardless of changes.
TIP:
You can configure this setting in .
FactoryTalk Linx Gateway
Configuration > MQTT > MQTT Client > MQTT Dataset (subscriber)> Subscriber
Properties > Tag Write ConfigurationLocation
- FactoryTalk Diagnostics Counter Monitor > System Diagnostics > localhost >FactoryTalk Linx GatewayMQTT Server > [Client ID] > [Dataset Name]
Value
- Type: Boolean
- Source: This value is generated by theFactoryTalk Linx GatewayMQTT service.
- Updates: This value updates when the MQTT configuration changes.
- Reset: This value resets when you reset the service or restart the computer.
Provide Feedback