Sub_Drop Items
Description
This value indicates the total number of dataset tags that the
FactoryTalk Linx Gateway
subscriber is unable to process due to resource limitations or configuration
constraints, such as queue overflow or high data arrival rates.For more information about the subscriber configuration, see
FactoryTalk Linx Gateway
Help.Location
- FactoryTalk Diagnostics Counter Monitor > System Diagnostics > localhost >FactoryTalk Linx GatewayMQTT Server > [Client ID] > [Dataset Name]
Value
- Type: 64-bit signed integer
- Source: This value is generated by theFactoryTalk Linx GatewayMQTT service.
- Updates: This value increases when the subscriber is unable to process the upcoming data due to resource limitations or configuration constraints.
- Reset: This value resets when you reset the service or restart the computer.
Provide Feedback