Sub_Dateset Name
Description
This value indicates the user-assigned dataset name configured in .
FactoryTalk Linx Gateway
Configuration > MQTT > MQTT Client > MQTT Dataset >
Dataset PropertiesLocation
- FactoryTalk Diagnostics Counter Monitor > System Diagnostics > localhost >FactoryTalk Linx GatewayMQTT Server > [Client ID] > [Dataset Name]
Value
- Type: String
- Source: This value is generated by theFactoryTalk Linx GatewayMQTT service.
- Updates: This value updates when the configuration changes in the MQTT dataset.
- Reset: This value resets when you reset the service or restart the computer.
Provide Feedback