Service Version

Description
This value indicates the version of the
FactoryTalk Linx Gateway
MQTT service. For example, 6.50.00.
TIP:
This value should match the product version in the Properties of the application.
Location
  • FactoryTalk Diagnostics Counter Monitor > System Diagnostics > localhost >
    FactoryTalk Linx Gateway
    MQTT Server
Value
  • Type: String
  • Source: This value is generated by the
    FactoryTalk Linx Gateway
    MQTT service.
  • Updates: This value is loaded when the service initially starts.
  • Reset: This value resets when you reset the service or restart the computer.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal