Service Status

Description
This value indicates the status of the
FactoryTalk Linx Gateway
MQTT service:
  • "Starting" indicates that the service is in the process of starting up.
  • "Running" indicates that the service is running and operational.
  • "Stopping" indicates that the service is in the process of shutting down.
  • "Stopped" indicates that the service has stopped and is not operational.
Location
  • FactoryTalk Diagnostics Counter Monitor > System Diagnostics > localhost >
    FactoryTalk Linx Gateway
    MQTT Server
Value
  • Type: String
  • Source: This value is generated by the
    FactoryTalk Linx Gateway
    MQTT service.
  • Updates: This value is loaded when the service initially starts.
  • Reset: This value resets when you reset the service or restart the computer.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal