Service Start Timestamp
Description
This value indicates the precise time at which the
FactoryTalk Linx Gateway
MQTT service starts.For example, ā2024-01-26T01:09:45.502Zā represents a connection established on January 26, 2024, at 1:09:45 AM and 502 milliseconds in Coordinated Universal Time (UTC).
Location
- FactoryTalk Diagnostics Counter Monitor > System Diagnostics > localhost >FactoryTalk Linx GatewayMQTT Server
Value
- Type: String
- Source: This value is generated by theFactoryTalk Linx GatewayMQTT service.
- Updates: This value is loaded when the service initially starts.
- Reset: This value resets when you reset the service or restart the computer.
Provide Feedback