Number of Clients
Description
This counter indicates the number of MQTT clients that are configured.
You can configure the MQTT client in .
FactoryTalk Linx Gateway
Configuration > MQTT > MQTT ClientLocation
- FactoryTalk Diagnostics Counter Monitor > System Diagnostics > localhost >FactoryTalk Linx GatewayMQTT Server
Value
- Type: 64-bit signed integer
- Source: This value is generated by theFactoryTalk Linx GatewayMQTT service.
- Updates: This value increases when an MQTT client is configured and decreases when it is removed.
- Reset: This value resets when you reset the service or restart the computer.
Provide Feedback