Pub_Valid Data Items
Description
This counter indicates the number of valid dataset tags configured in the
FactoryTalk Linx Gateway
MQTT publisher.
TIP:
The value will not exceed the current activation limit.
Location
- FactoryTalk Diagnostics Counter Monitor > System Diagnostics > localhost >FactoryTalk Linx GatewayMQTT Server > [Client ID] > [Dataset Name]
Value
- Type: 64-bit signed integer
- Source: This value is generated by theFactoryTalk Linx GatewayMQTT service.
- Updates: This value updates when the configuration in the MQTT publisher changes.
- Reset: This value resets when you reset the service or restart the computer.
Provide Feedback