Pub_Topic

Description
This counter indicates the user-assigned topic name, which identifies the information channel to which payload data is published.
You can configure the topic name in
FactoryTalk Linx Gateway
Configuration > MQTT > MQTT Client > MQTT Dataset > Dataset Properties
.
Location
  • FactoryTalk Diagnostics Counter Monitor > System Diagnostics > localhost >
    FactoryTalk Linx Gateway
    MQTT Server > [Client ID] > [Dataset Name]
Value
  • Type: String
  • Source: This value is generated by the
    FactoryTalk Linx Gateway
    MQTT service.
  • Updates: This value updates when the configuration changes in the MQTT dataset.
  • Reset: This value resets when you reset the service or restart the computer.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal