Pub_Retain
Description
This value indicates if the MQTT broker retains the messages from the publishers.
You can configure the setting in .
FactoryTalk Linx Gateway
Configuration > MQTT > MQTT Client > AdvanceThere are two values:
- “Yes” indicates that the retain function is enabled.The MQTT broker will store the latest messages from the publishers.
- “No” indicates that the retain function is disabled.The MQTT broker will not store messages from the publishers.
Location
- FactoryTalk Diagnostics Counter Monitor > System Diagnostics > localhost >FactoryTalk Linx GatewayMQTT Server > [Client ID] > [Dataset Name]
Value
- Type: String
- Source: This value is generated by theFactoryTalk Linx GatewayMQTT service.
- Updates: This value updates when the configuration changes in the MQTT client.
- Reset: This value resets when you reset the service or restart the computer.
Provide Feedback