Pub_Publishing Interval (ms)

Description
This counter indicates the frequency (in milliseconds) at which the MQTT clients send data to the broker. The default value is 1000.
You can configure the publishing intervals in
FactoryTalk Linx Gateway
Configuration > MQTT > MQTT Client > MQTT Dataset > Dataset Properties
.
Location
  • FactoryTalk Diagnostics Counter Monitor > System Diagnostics > localhost >
    FactoryTalk Linx Gateway
    MQTT Server > [Client ID] > [Dataset Name]
Value
  • Type: 64-bit signed integer
  • Source: This value is generated by the
    FactoryTalk Linx Gateway
    MQTT service.
  • Updates: This value updates when the configuration changes in the MQTT dataset.
  • Reset: This value resets when you reset the service or restart the computer.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal