Pub_Payload Format

Description
This value indicates the format in which the payload of messages is structured.
  • FactoryTalk Optix Format
  • Rich Format
  • Flat Format
You can configure this setting in
FactoryTalk Linx Gateway
Configuration > MQTT > MQTT Client > Advance
.
For more information on the payload format, see
FactoryTalk Linx Gateway
Help
.
Location
  • FactoryTalk Diagnostics Counter Monitor > System Diagnostics > localhost >
    FactoryTalk Linx Gateway
    MQTT Server > [Client ID] > [Dataset Name]
Value
  • Type: String
  • Source: This value is generated by the
    FactoryTalk Linx Gateway
    MQTT service.
  • Updates: This value updates when the configuration changes in the MQTT client.
  • Reset: This value resets when you reset the service or restart the computer.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal