Pub_Max Payload Size (kB)
Description
This counter indicates the maximum size for the payload of a message in kilobytes. The default value is 1000. The supported range is from 1 through 200,000.
You can configure this value in .
FactoryTalk Linx Gateway
Configuration > MQTT > MQTT Client > AdvanceLocation
- FactoryTalk Diagnostics Counter Monitor > System Diagnostics > localhost >FactoryTalk Linx GatewayMQTT Server > [Client ID] > [Dataset Name]
Value
- Type: 64-bit signed integer
- Source: This value is generated by theFactoryTalk Linx GatewayMQTT service.
- Updates: This value updates when the configuration changes in the MQTT client.
- Reset: This value resets when you reset the service or restart the computer.
Provide Feedback