Pub_Invalid Data Items
Description
This counter indicates the number of dataset tags requested by the
FactoryTalk Linx Gateway
MQTT publisher that were not activated because they exceeded
the current activation limit.
TIP:
The total number of publisher and subscriber tags
cannot exceed the
FactoryTalk Linx Gateway
activation.Location
- FactoryTalk Diagnostics Counter Monitor > System Diagnostics > localhost >FactoryTalk Linx GatewayMQTT Server > [Client ID] > [Dataset Name]
Value
- Type: 64-bit signed integer
- Source: This value is generated by theFactoryTalk Linx GatewayMQTT service.
- Updates: This value updates when the configuration in the MQTT publisher changes.
- Reset: This value resets when you reset the service or restart the computer.
Provide Feedback