Pub_Failed to Deliver Data

Description
This counter indicates the total number of messages that the MQTT publisher attempted to send to the broker but were not successfully delivered.
Location
  • FactoryTalk Diagnostics Counter Monitor > System Diagnostics > localhost >
    FactoryTalk Linx Gateway
    MQTT Server > [Client ID] > [Dataset Name]
Value
  • Type: 64-bit signed integer
  • Source: This value is generated by the
    FactoryTalk Linx Gateway
    MQTT service.
  • Updates: This value increases when a message sent from the MQTT publisher to the broker fails.
  • Reset: This value resets when you reset the service or restart the computer.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal