Pub_Deliver Data
Description
This counter indicates the total number of messages sent by the MQTT publisher to the
broker.
Location
- FactoryTalk Diagnostics Counter Monitor > System Diagnostics > localhost >FactoryTalk Linx GatewayMQTT Server > [Client ID] > [Dataset Name]
Value
- Type: 64-bit signed integer
- Source: This value is generated by theFactoryTalk Linx GatewayMQTT service.
- Updates: This value increases when the MQTT publisher successfully sends a message to the broker.
- Reset: This value resets when you reset the service or restart the computer.
Provide Feedback