Pub_Data Content
Description
This value indicates the attributes included in the dataset, such as Tag Name, Value, Timestamp, Quality, and Data Type. You can configure this setting in .
FactoryTalk Linx Gateway
Configuration > MQTT > MQTT Client > MQTT Dataset > Dataset Properties
TIP:
Tag Name and Value are selected by default and cannot be edited.
For example, if Quality and Data Type are selected, the value will display as “Tag Name; Value; Quality; Data Type”.
Location
- FactoryTalk Diagnostics Counter Monitor > System Diagnostics > localhost >FactoryTalk Linx GatewayMQTT Server > [Client ID] > [Dataset Name]
Value
- Type: String
- Source: This value is generated by theFactoryTalk Linx GatewayMQTT service.
- Updates: This value updates when the configuration changes in the MQTT dataset.
- Reset: This value resets when you reset the service or restart the computer.
Provide Feedback