Service Certificate
Description
This value specifies the path where outgoing public certificates are stored on the computer running
FactoryTalk Linx Gateway
. These outgoing public certificates will be transmitted to MQTT clients upon connection.Location
- FactoryTalk Diagnostics Counter Monitor > System Diagnostics > localhost >FactoryTalk Linx GatewayMQTT Server > [Client ID]
Value
- Type: String
- Source: This value is generated by theFactoryTalk Linx GatewayMQTT service.
- Updates: This value is loaded when the service initially starts.
- Reset: This value resets when you reset the service or restart the computer.
Provide Feedback