Received Messages
Description
This counter tracks the total number of MQTT messages received by all
FactoryTalk Linx Gateway
MQTT subscribers from the third-party MQTT brokers.Location
- FactoryTalk Diagnostics Counter Monitor > System Diagnostics > localhost >FactoryTalk Linx GatewayMQTT Server > [Client ID]
Value
- Type: 64-bit signed integer
- Source: This value is generated by theFactoryTalk Linx GatewayMQTT service.
- Updates: This value increases when the MQTT subscriber successfully receives an MQTT message from the broker.
- Reset: This value resets when you reset the service or restart the computer.
Provide Feedback