Rejected Connections
Description
This value indicates the number of connection attempts rejected between the MQTT client
and the broker.
Location
- FactoryTalk Diagnostics Counter Monitor > System Diagnostics > localhost >FactoryTalk Linx GatewayMQTT Server > [Client ID]
Value
- Type: 64-bit signed integer
- Source: This value is generated by theFactoryTalk Linx GatewayMQTT service.
- Updates: This value increases when the MQTT broker rejects the MQTT client 's connection attempt.
- Reset: This value resets when you reset the service or restart the computer.
Provide Feedback