Number of Datasets

Description
This counter indicates the number of the datasets established by the MQTT client.
Location
  • FactoryTalk Diagnostics Counter Monitor > System Diagnostics > localhost >
    FactoryTalk Linx Gateway
    MQTT Server > [Client ID]
Value
  • Type: 64-bit signed integer
  • Source: This value is generated by the
    FactoryTalk Linx Gateway
    MQTT service.
  • Updates: This value increases when an MQTT dataset is created and decreases when it is removed.
  • Reset: This value resets when you reset the service or restart the computer.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal