Last Rejected Connection Message
Description
This value indicates the message from the third-party MQTT broker explaining the reason
for the most recently rejected MQTT client connection attempt.
Location
- FactoryTalk Diagnostics Counter Monitor > System Diagnostics > localhost >FactoryTalk Linx GatewayMQTT Server > [Client ID]
Value
- Type: String
- Source: This value is generated by the third-party MQTT broker.
- Updates: This value is loaded when the MQTT broker rejects the MQTT client's connection attempt.
- Reset: This value resets when you reset the service or restart the computer.
Provide Feedback