Last Connection Timestamp

Description
This value indicates the time of the most recent connection between the MQTT client and the broker.
For example, ā€œ2025-01-26T01:09:45.502Zā€ represents a connection established on January 26, 2025, at 1:09:45 AM and 502 milliseconds in local time.
Location
  • FactoryTalk Diagnostics Counter Monitor > System Diagnostics > localhost >
    FactoryTalk Linx Gateway
    MQTT Server > [Client ID]
Value
  • Type: String
  • Source: This value is generated by the
    FactoryTalk Linx Gateway
    MQTT service.
  • Updates: This value is loaded when the MQTT client connects to the broker.
  • Reset: This value resets when you reset the service or restart the computer.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal