Enable SSL/TLS
Description
This value indicates whether the SSL/TLS encryption is enabled in .
FactoryTalk Linx Gateway
Configuration > MQTT > MQTT Client > SecurityThere are two values:
- “Yes” indicates that SSL/TLS encryption is enabled.
- “No” indicates that SSL/TLS encryption is disabled.
Location
- FactoryTalk Diagnostics Counter Monitor > System Diagnostics > localhost >FactoryTalk Linx GatewayMQTT Server > [Client ID]
Value
- Type: String
- Source: This value is generated by theFactoryTalk Linx GatewayMQTT service.
- Updates: This value updates when the configuration changes in the MQTT client.
- Reset: This value resets when you reset the service or restart the computer.
Provide Feedback