Connection Status

Description
This value indicates the connection status between the broker and the MQTT client configuration that you created in
FactoryTalk Linx Gateway Configuration > MQTT
.
  • “Connected” indicates that the current MQTT client is connected to the broker.
  • “Disconnected” indicates that the current MQTT client is not connected to the broker.
Location
  • FactoryTalk Diagnostics Counter Monitor > System Diagnostics > localhost >
    FactoryTalk Linx Gateway
    MQTT Server > [Client ID]
Value
  • Type: String
  • Source: This value is generated by the
    FactoryTalk Linx Gateway
    MQTT service.
  • Updates: This value reflects the connection status between the clients and the broker.
  • Reset: This value resets when you reset the service or restart the computer.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal