Connected IP Address

Description
This value indicates the IP address or host name of the MQTT broker. For example, “localhost” or “127.0.0.1” if the broker and clients are on the same computer.
You can configure the IP address in
FactoryTalk Linx Gateway
Configuration > MQTT > MQTT Client > Connection
.
Location
  • FactoryTalk Diagnostics Counter Monitor > System Diagnostics > localhost >
    FactoryTalk Linx Gateway
    MQTT Server > [Client ID]
Value
  • Type: String
  • Source: This value is generated by the
    FactoryTalk Linx Gateway
    MQTT service.
  • Updates: This value updates when the configuration changes in the MQTT client.
  • Reset: This value resets when you reset the service or restart the computer.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal