Authentication
Description
This value indicates whether to use a secured connection to the third-party MQTT broker.
You can configure the setting in .
FactoryTalk Linx Gateway
Configuration > MQTT > MQTT Client > Security > SSL/TLS > User Authentication- IfUser Authenticationis cleared, the value is “None”, indicating that the connection is made without user authentication.
- IfUser Authenticationis selected, the value corresponds to the username configured inUser Authentication.
Location
- FactoryTalk Diagnostics Counter Monitor > System Diagnostics > localhost >FactoryTalk Linx GatewayMQTT Server > [Client ID]
Value
- Type: String
- Source: This value is generated by theFactoryTalk Linx GatewayMQTT service.
- Updates: This value updates when the configuration changes in the MQTT client.
- Reset: This value resets when you reset the service or restart the computer.
Provide Feedback