FactoryTalk Linx Gateway MQTT diagnostics values

The following internal diagnostic values, counters and strings are made available by
FactoryTalk Linx Gateway
MQTT service for diagnostic purposes. These diagnostic values track activity at the boundary between the
FactoryTalk Linx Gateway
's MQTT client and the MQTT broker, and they are supported by FactoryTalk Diagnostics Counter Monitor.
The diagnostic counters display values since the
FactoryTalk Linx Gateway
MQTT service initially starts. The diagnostic counters are reset only when the service is stopped and restarted.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal