Service Status
Description
This value indicates the status of the FactoryTalk Linx Gateway DDE service.
- RUNNING: indicates that the service is running and operational.
TIP:
The FactoryTalk Linx Gateway DDE service has multiple states, including starting, running, stopping, and stopped. However, in Diagnostics Counter Monitor, only running will be shown under the Service Status counter. If the service isn’t in the running state, this counter will not appear.
Location
- FactoryTalk Diagnostics Counter Monitor > System Diagnostics > localhost > FactoryTalk Linx Gateway DDE Server
Value
- Type: String
- Source: This value is generated by the FactoryTalk Linx Gateway DDE server.
- Updates: This value is loaded when the service initially starts.
- Reset: This value resets when you reset the service or restart the computer.
Provide Feedback