LicenseName
Description
The FactoryTalk Linx Gateway DDE server obtains the activation from the FactoryTalk Activation Manager. The value indicates the name of the activation in use. If no activation is found, it displays “Activation not found”.
Location
- FactoryTalk Diagnostics Counter Monitor > System Diagnostics > localhost > FactoryTalk Linx Gateway DDE Server
Value
- Type: String
- Source: This value is generated by the FactoryTalk Linx Gateway DDE server.
- Updates: This value is loaded when the service initially starts.
- Reset: This value will be retrieved when you reset the service or restart the computer.
Provide Feedback