Count against Activation

Description
This value indicates the number of tags that have been added to the server. This number includes active and inactive tags. Duplicate tags count as a single tag.
TIP:
Count against Activation provides a real-time tag count rather than an accumulated value since the service started. The value will change as tags are added or removed.
Location
  • FactoryTalk Diagnostics Counter Monitor > System Diagnostics > localhost > FactoryTalk Linx Gateway DDE Server
Value
  • Type: Unsigned integer
  • Source: This value is generated by the FactoryTalk Linx Gateway DDE server.
  • Updates: This value increases when a DDE client adds a new tag and decreases when removing an existing tag.
  • Reset: This value resets when you reset the service or restart the computer.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal