Client Disconnect calls

Description
This counter indicates the number of times that FactoryTalk Linx Gateway DDE server has received disconnection requests from the DDE clients.
TIP:
If the FactoryTalk Linx Gateway Configuration dialog is closed, the Client Disconnect Calls count will increment.
Location
  • FactoryTalk Diagnostics Counter Monitor > System Diagnostics > localhost > FactoryTalk Linx Gateway DDE Server
Value
  • Type: Unsigned integer
  • Source: This value is generated by the FactoryTalk Linx Gateway DDE server.
  • Updates: This value increases when a DDE client disconnects from the FactoryTalk Linx Gateway DDE server.
  • Reset: This value resets when you reset the service or restart the computer.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal