Client Call OnRequest

Description
This counter indicates the number of times that the DDE client made to request the data item from the FactoryTalk Linx Gateway DDE server using the OnRequest transaction type.
Location
  • FactoryTalk Diagnostics Counter Monitor > System Diagnostics > localhost > FactoryTalk Linx Gateway DDE Server
Value
  • Type: Unsigned integer
  • Source: This value is generated by the FactoryTalk Linx Gateway DDE server.
  • Updates: This value increases when a DDE client requests the data item using the OnRequest transaction type.
  • Reset: This value resets when you reset the service or restart the computer.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal