Client Call OnPoke
Description
This counter indicates the number of requests that the DDE client made to send unsolicited data to the FactoryTalk Linx Gateway DDE server using the OnPoke transaction type.
Location
- FactoryTalk Diagnostics Counter Monitor > System Diagnostics > localhost > FactoryTalk Linx Gateway DDE Server
Value
- Type: Unsigned integer
- Source: This value is generated by the FactoryTalk Linx Gateway DDE server.
- Updates: This value increases when a DDE client requests the data item using the OnPoke transaction type.
- Reset: This value resets when you reset the service or restart the computer.
Provide Feedback