Client call OnAdvStart
Description
This counter indicates the number of requests the DDE client made to start an advise loop with the FactoryTalk Linx Gateway DDE server using the OnAdvStart transaction type. It shows how many times the DDE client asked to get updates about an item from the FactoryTalk Linx Gateway DDE server.
Location
- FactoryTalk Diagnostics Counter Monitor > System Diagnostics > localhost > FactoryTalk Linx Gateway DDE Server
Value
- Type: Unsigned integer
- Source: This value is generated by the FactoryTalk Linx Gateway DDE server.
- Updates: This value increases when a DDE client requests the data item using the OnAdvStart transaction type.
- Reset: This value resets when you reset the service or restart the computer.
Provide Feedback