ShelvingState

Description
Suggests whether an alarm is temporarily be prevented from being displayed to the user.
UnshelveTime
Description
Specifies the remaining time in milliseconds before the alarm automatically transitions into the unshelved state.
Data Type
VT_LPWSTR
For more information, refer to FiniteStateMachineType.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal